HI all,
I want to make sure something, right now I am checking the I2C LOG of the LED Driver
1. whether the placement is correct between the Brightness path diagram and the diagnostic register below?
And where is the correct path for Brightness control
2. In hybrid mode, it combined the Current mode and PWM Mode, i would like to ask, for the PWM Mode, it is start from the Duty Cycle 12.5% OR <25%?
And in PWM Mode, the current shouldn't be change right?
Thank you