This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25173-Q1: thermal protection

Part Number: BQ25173-Q1

Hi colleagues,

If I have fully discharged supercap 0V and 16V as input I have 800mA set, I have 12.8W on this LDO. I think that we would run fast into a thermal protection situation since the thermal impedance is 71°C/W. What is the behavior of this device? Thermal protection?

Thank you,

Daria