This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2595: minimum measurable load current on ILIM pin

Part Number: TPS2595
Other Parts Discussed in Thread: TPS2596, TPS1641, TPS25961

Dear all

I'm designing a board that has to work at 3V, 150mA max and any current over 250mA is considered a shortcircuit

On the other hand, I have to monitor the current that the board draws. I thought in using the ILIM pin to monitor the

board's current, but, after reading the TPS259530DSG DS I've found that the ILIM resistor voltage is a bit imprecise.

I need to know what is the lowest attainable measured load current on ILIM pin, or if I have to change the efuse part for 

a more proper one.

Thanks in advance

Ignacio