Hi Team,
I would like to double check for the following questions:
1. Flags register (0x05) UVLO Fault was triggered, is it possible to clear this register bit by cut off LM36010 input power[No input power]?
2.What is the triggering logic of UVLO Fault? How long can it trigger UVLO Fault when Vin is less than 2.5V? A power down also makes VIN less than 2.5V, so why does UVLO not trigger?
3.Can we turn off flash mode by pulling down STROBE pin? If not, what is the reason for it.
Thanks
Frank