Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54308: TPS54308: BOOTSTAP

Part Number: TPS54308

Hi All,

I am using the TPS54308 for a 24V to 5V design.

All my calculations converge to the simulations and all is perfect except one thing.

in the DS, it says that BOOT-SW voltage should be -0.3V to 7V.

Looking at the DS and the internal design of TPS54308 it looks like this voltage is something internally
and my responsibility is to provide the needed capacitor to store the needed energy.

in the simulation I measure 25.8 Volt which is way higher than 7V.
what's is the cause ? how can i fix it?


 tina_ti_imulation - autosave 24-04-11 12_49 - autosave 24-04-16 09_32.TSC