Other Parts Discussed in Thread: TPS2113, TPS2216, TPS2121, TPS2115A
Hi
The ideal mode should be the diode mode so that the battery with the highest voltage is active. It will work in standalone mode.
However, the datasheet (page 11) suggests not using that mode for this configuration:" It is not recommended to use diode operation for two inputs of the same voltage, that is when the device is to multiplex and to connect one input channel to the output. "
Why is it not recommended?
Are there any other suggested devices or configurations?
During the crossover between batteries, the load should continue working. Is it necessary to add a large output capacitor to avoid dropout during the change between channels?
Thanks