Other Parts Discussed in Thread: LM5069
Hi TI,
I am planning to use 2x LM5066I configured in back-to-back similar to the attached schematic. I would like to use the controls and protections (OCP, OVP, UVLO) for bidirectional current. I am designing for 16A at +48V
1) Is this configuration OK for LM5066I eFuse, with external N-FET? I am going to use 2x Linear FET IPB017N10N5LF in common source configuration, each MOSFET connected to each eFuse GATE pin.
2) LM5066I has I2C for telemetry and it can only read positive current through its I2C. With this configuration, I believed I can use one eFuse for current reading through I2C for each of the current direction (I will need to handle the direction of the current flow, and I can do this in my microcontroller). What will happen to the I2C current reading for the eFuse that has reverse current though it, since it can only read forward current? Will the register saturated at 0 or some other value?
Thanks