Part Number: LM5146
Other Parts Discussed in Thread: LM5145, , CSD19531Q5A, LM25148
Hi,
I need help in getting schematic review for the board design.
Can someone help me with it?
I need it ASAP
Thanks
8154.schematic.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM5146
Other Parts Discussed in Thread: LM5145, , CSD19531Q5A, LM25148
Hi,
I need help in getting schematic review for the board design.
Can someone help me with it?
I need it ASAP
Thanks
8154.schematic.pdf
Hi Bob,
Apologies for the delay.
Here are some comments:
Regards,
Tim
Can you share with me exact part number for it plz?
Regarding you 1st message, I used webench and EVM design files to create this schematic. I will look another link as well..
Can you elaborate 4th point further please?
I also need layout review after it.
Thanks
LM5145RGYR, see https://www.ti.com/product/LM5145#order-quality
You can use Murata's tool to check the effective capacitance of the ceramic at a given voltage: https://ds.murata.co.jp/simsurfing/mlcc.html?lcid=en-us&jis=false
Here is the plot for a 22uF/25V/1210/X7R at room temp:

Hi Timothy Hegarty
I guess, LM5146 is fine considering future use because i don't see any reason to choose LM5145 over 46.
Second, I need to know why i have to choose different MOSFETs for High and LOW side. Can you help me to understand it?
I noticed in the Webench that they are different.
I want to use low cost MOSFET but if I use HIGH side CSD19531Q5A then Webench suggest SUM90N10-8M2P-E3. This MOSFET is not only expensive but different package as well.
I tried to use NexFET selector tool but I couldn't understand it much. It has different GUI than the video available for it.
The output capacitors that I used is C3216X5R1V226M160AC from TDK.
I got your point about its effective capacitance.
Can you suggest some solution for it please?
I checked at Webench. It change the capacitance values
8.4V = 22uF
12.6V = 2x 22uF
16.8V = 3x10uF
Thanks
Hi Bob,
The LM5145 is lower cost, hence that suggestion. They are pin-to-pin compatible, so you could change in future as well if needed.
In terms of the MOSFETs, the high-side FET has all the switching loss, so higher Rdson (lower capacitance) is possible. And the low-side FET is conduction loss dominant, especially for large step-down ratios, so it can be lower Rdson. I would stick with 5 x 6mm MOSFETs - take a look at the LM5146 EVM, which is a 12V/8A/400kHz design (close to your spec).
The LM5146 quickstart calculator will be really helpful for your design - please complete and send that for review.
--
Tim
In terms of output caps, I recommend using 22uF/25V/X7R/1210. The total effective capacitance will be lowest at the highest Vout setting, so design the compensation for that and then do a quick check at the lower output voltages with those values.
--
Tim
Hi Timothy Hegarty
I added the values according to the requirements and some values that i already used in the circuit. For example, compensation circuit.
I have no idea about pole and zero that you might adjust it.
I have different battery power sources so i selected minimum voltages consider low battery cell count and Nominal/Max considering higher cell count.
I setup current limit to 12A that was previously i guess set at 25A.
Now here is the tricky part because, the output will change i.e. 8.4V/12.6V/16.8V
I attached all the sheets for various output. Plz, have a look and let me know if i missed anthing.
I will use then final sheet BOM that you will suggest.
16.8V.xlsm12.6V.xlsm8.4v.xlsm
Last, If this is your email then I have another request also pending on your end at TI customer support. Plz, confirm me if it is yours.
Tim.Hegarty@ti.com
Thanks
Hi Bob,
Let me check email for the layout.
Are these 3 separate designs or just one with adjutable Vout? If it's the latter, then we design the compensation with highest Vout (lowest effective Cout) and then check the lower voltages with the compensation values fixed.
--
Tim
These are same design but i adjusted Vout differently in all three.
I also noticed in other buck design that most of the time(Even reference design and Webench Design) used same MOSFET for High and Low side.
This is my email for layout review of LM25148 that i sent you few weeks ago.
ali.khan@brainchildengineering.com
Three different output voltage but one implementation - so it has an adjustable Vout, correct? Just wondering if we need to have one compensation network for all three, or if we can optimize it for each Vout setting.
Yes correct.
I need 3 different outputs select able through a switch.
I need one network for all because i don't want to add more components for each setting.
There should be one optimal solution that can do all three.
It's like adjustable buck converter and I found many in the market
Just looking at the quickstarts, I see you are not adjusting Cout for the different output voltages. Go ahead and insert the correct "effective Cout" for each output voltage setpoint, and keep the compensation network constant based on the stability for the highest Vout.
Just looking at the quickstarts, I see you are not adjusting Cout for the different output voltages. Go ahead and insert the correct "effective Cout" for each output voltage setpoint, and keep the compensation network constant based on the stability for the highest Vout.
Also, you may use 80V FETs here for better efficiency. No need for 100V device if the layout is good and Vin-max is only 65V.
I found the layout. Here are some comments:
Hi Bob,
This still shows 22uF for 8.4Vout, but it should give the highest capacitance based on the derating with voltage of ceramics.

My assumption is you're selecting a set of capacitors that will work with this adjustable output design, so just enter the applicable capacitance for the three Vout levels. Actually, we usually just check min and max Vout -- design the loop for max Vout and fix the compensation values when checking the min Vout with the higher effective Cout value.
--
Tim
Hi Timothy Hegarty
I sent you an email for layout review of this design.
Plz, check that and Let me know if you need anything futher.
Also,
I need some guides related to buck converter that i can follow up in the future design.
I actually design many buck/boost converter and I feel like missing many aspects from design perspective.
Last but not least,
Where i can learn about the following.
1: Compensation Circuit,
2: Pole and Zero placement
3: Crossover Frequency
4: Input/Output capacitor selection
I checked datasheet. It has some equations.
Are there some thumb rules that i can follow to design TI based buck converters.
Thanks for all your help.
I really appreciate it.
Hi Bob,
The LM5145 / LM5146 datasheet actually has some good info on compensation for voltage-mode control. I have a couple of articles on how2power.com on current-mode control as well that are worth looking at.
I'll check my inbox now to see if I got your latest layout. The LM5145 and LM5146 EVMs are actually good templates to copy from a layout standpoint. Also, the datasheet guidelines for layout are pretty comprehensive.
Regards,
Tim
Plz confirm me if you are able to find layot files in email.
It would be great if you can give me some feedback before next week.
Thanks
Hi Timothy Hegarty
It would be great if you can give me feedback today.
I am a bit getting late on production cycle.
Thanks
Hi Bob,
Here are some comments upon reviewing "Voltage limiter V1":
Tim
Also, take a look at the LM5145 EVM layout for reference. The LM5145 is effectively the same controller as the LM5146, just a lower Vin-max rating.
Hi Timothy Hegarty
Thanks for your feedback.
I will update the design of LM5146 based on all these valuable suggestions.
It cleared a lot of my concept.
I need one final request if you can help me with it plz.
It is about LM25148.
You mentioned that i should use sense resistor different size.
Can you help me to fill out this CAL for the following parameters.
1: Priority small size inductor and board size
2: Vin 10 to 36V
3: Vout 7.4V 15A
The height of the components should be minimize as well. The major component that drive height and all parameter is inductor.
I tried to follow up WEBENCH and other recommendation but due to board size it is not feasible for me
LM5148-LM25148 Quickstart Calculator_rev2.xlsm
https://webench.ti.com/power-designer/switching-regulator/customize/103?VinMin=9&VinMax=36&O1V=7.4&O1I=12&base_pn=LM25148&AppType=None&Flavor=None&op_TA=30&origin=pf_panel&lang_chosen=en-US&optfactor=3&Topology=Buck&flavor=None&VoltageOption=None
Hi Bob,
What you have looks pretty good for the LM25148. Just drop the shunt to 3mΩ, so you have some margin from full load to current limit. We typically recommend 125-150%, so you could even drop it to 2mΩ. Also, you can go with a 2.2uH inductor, which is a standard value - take a look at Coilcraft XGL series of inductors. The output cap ESR should be a few mΩ if you use ceramics.
I recommend submitting a separate E2E for the LM25148 if you need further support - then the responsible engineer will reply.
Regards,
Tim