Part Number: UCC28065
Other Parts Discussed in Thread: UCC28070A, , UCC28070
Hi Team,
Could you help recommend best solution for FAN9673Q? I only find two ch Interleaved CCM.
Thank you!
Marc
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Marc,
The UCC28070A 2-channel interleaved CCM PFC controller is the best alternative to the FAN9673Q device.
We do not have a 3-channel analog controller, although one can be constructed using a digital controller such as the C2000 MCU (ref: https://www.ti.com/tool/PMP40690 ).
The UCC28065 that you reference in the E2E title is a 2-channel interleaved Transition-Mode PFC controller. It does not operate in CCM.
3 channels of interleaving does not necessarily provide a great advantage over 2 interleaved channels. Mostly, it disperses the losses more widely and reduces component volume somewhat at the expense of higher BOM count and costs.
This white paper: https://www.ti.com/lit/pdf/slua746 shows in Figure 10 that 2 channel interleaving provides 100% cancellation (0% ripple) when the duty cycle is 50% which is where the current ripple peak-to-peak magnitude is highest. 3-channel interleaving provides 100% cancellation at ~0.33 and ~0.66 duty, but the actual ΔI at those points are already lower. And it only cancels about 70% at the highest ΔI at duty = 0.5.
Also the UCC part is less than 1/2 the cost of the FAN device, while retaining most of the basic functions.
And two UCC28070 controllers can be easily paralleled to provide 4-phase interleaving, if desired, which retains 100% ripple cancellation at max ΔI as well as lower remaining ripple.
Regards,
Ulrich