Other Parts Discussed in Thread: UCC5390
Hi,
I would like to know if TI's isolated gate driver can handle system abnormalities.
System configuration
・When normal operation: output side VCC withstand voltage is 40V and 20V is applied to VCC2.
・When normal operation: 15V is applied to the IGBT gate with negative bias of 5V.
・When an error occurs: 30V is applied to the output side VCC due to an error in the power supply circuit in the previous stage.
・When an error occurs: 25V is applied to the IGBT gate with a negative bias of 5V (gate breakdown voltage exceeds 20V)
Question
Is there a lineup of isolated gate drivers that can take measures against overvoltage to the IGBT gate during abnormal conditions? The following functions are expected.
■Detects unintended voltage on the insulated gate driver side and stops gate output
■The output of the insulated gate driver contains a constant voltage circuit and only outputs 15V. etc.
Thanks,
Conor