Other Parts Discussed in Thread: BQ27Z561
Hi,
I am currently in the process of configuring the necessary parameters to initiate the learning cycle. However, I am encountering challenges in obtaining the correct values for the below mentioned parameters.
- Charge current threshold
- Discharge current threshold
- Charge term taper current
- Quit current
A critical condition for a successful learning cycle is to ensure that the charge current threshold is less than the termination taper current and quit current. Despite my efforts, I am struggling to determine the appropriate value for the charge term taper current.
The battery which I am using for my training process is LP353035 with 400mAh having typical voltage of 3.7V.
I have experimented with various resistor values which is connected to the JP9 connector in the EVM, each yielding different results:
- Resistor with 40.2K: In this scenario, the current dropped to zero from 400mA.
- Resistor with 150K: I encountered difficulty in obtaining complete logs of the average current.
- Resistor with 220K: Difficulty in obtaining complete logs of the average current.
- Resistor with 300K: In this case, the current dropped to zero from 131mA within one second, despite the required elapsed time being 80 seconds.
Given the above observations, what changes I need to make to obtain the correct parameters for the learning cycle.
I am attaching the log files of all the four experiments I did, please go through it.
charging_40.2K.logcharging_150K.logcharging_220K.logcharging_300k.log
Thanks,
Ruchika