Hi there,
I utilize the diagram shown below; the document is attached.
My constant current range is 1 mA to 24 mA on the SENS_Pressure Sensor_InLo1 and SENS_Pressure Sensor_InHi1 pins.
Why does the DCP010515DB-U's voltage decrease at 24 mA from 30 V to 25 V?
I take this to mean that when I put the datasheet's stated current of Iout1+Iout2=66mA in series, I get 33mA (1W/30V=33mA).
I appreciate your assistance.