This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A80: TPS7A80 pin 6 (NR) output voltage fluctuates after being touched by hand

Part Number: TPS7A80

As described in the title, the output voltage of the TPS7A80 voltage regulator fluctuates after being touched by hand.

The input voltage is 5V and the output voltage is 3.3V.

However, if the output pin (pin 6) is touched by a baby's hand, the output voltage rises to 4.5V.