Other Parts Discussed in Thread: BQ25638, BQ25185, BQ24650, BQ25504
Please help with the selection,
Requirement:
1. Solar panel input voltage: 4.5V or above (standard 5V)
2. Single section lithium battery charging, with a standard lithium voltage of 3.6V and a maximum of 4.2V, and a charging current of 500mA or more.
3. With MPPT function
4. Equipped with protection functions such as input low-voltage shutdown protection, recharging, overcurrent protection, etc.
There is a demand of 4KK per year
Special requirements:
The charging IC for solar charging MPPT. The battery is mounted on the charging IC
Is the POWer pass function available? If my charging chip is not working, can the battery supply power to the module? The average power consumption of the module is 100-200mA, and when the power consumption is high, it can reach 2-3A,
Is it possible to supply 2-3 A of power to the system, regardless of whether it is in a charging state?
BQ25570RGRT、BQ25505RGRT、BQ24650RVAR、TI-BQ25504、TI-BQ25505 According to my request, which chip would be the most suitable and cost-effective option to choose?