Part Number: BQ27Z561-R2-DEVICE-FW
Other Parts Discussed in Thread: ADS1285EVM-PDK, ADS1285
I'm testing the ADS1285EVM-PDK 32bits ADC board, but I met some problems. When I only connect the UBS wire to PC and do not connect sonser, I measure the voltage of "+" pin (positive pin) and "-" pin (negtive pin) of IN 1 that are same (the value is +2.5 V) while the voltage of GND of IN1 is zero, which is strange. In my view, the volgage of "+" pin and "-" pin is inverse.
Another question is when I connect a sensor (the sensor is JAE JA-40GA Accelerometer who has a yellow signal wile labled "signal " and a white signa lwire labled " signal return" acutally connected to ground ) to IN 1 as the bellow manner: JAE " signal" wire to "+" pin of IN1, and JAE " signal return " wire to "-" pin of IN1, the measured singal is fluctuaded from zere to the acutall value( for example 1.05V). If I change the conncet manner (connect JAE " signal return" wire to "GND" pin of IN1) , the measured signal is 1.45 V (2.5 V-1.05 V =1.45 V ) whose rms noise is even worse than I measured using 24 bits NI 9239 borad. But when I have a self-noise test and mesure the self DAC singal of ADS 1285 board, the self-noise and test signal is ok.
Idon't know how to solve theose problems. Could you help me and give some advices.Thanks.