My customer was using LMR14050 for the below application:
Vin=24V, Vout=12V/ 2A.
They found the voltage output showed some unexpected ripple/spike during the soft start, with full load startup.
The issue was found if using the CC mode for the electrical load, and it did not show up if using CR mode. But their system tests all required CC mode setting.
Could you please help check the possible suggestions for them?
The inductor they used is 12uH.