Other Parts Discussed in Thread: LMG2610, UCC28782, UCC28600, UCC28740
Customer is wondering to know if UCC28782 + LMG2610 is able to realize below condition?
Pri : 127~373Vdc to
Sec: Vcc 5V/0.8A, Power = 4W
Sec: 40V~52V(48V) 16W (x 4), total power = 16x4 =64W
Total Power: 68W
Application: Aux Power for Servo Drive
Ambient Temp: 80degree
Or is there suited solution? Thanks.
Regards
Brian