This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR33630-Q1: design question about PG pin

Part Number: LMR33630-Q1
Other Parts Discussed in Thread: TPS745

Hi Sir,

My customer has a question about the power good function for LMR33630-Q1.

Follow the d/s 8.3.1 mentioned, the customer's design application as below.

The Ven is Vin/2, when Vin drops to 5V, the Ven = 2.5V > 2V. (power good remains valid as long as the input voltage is ≥ 2 V (typical))

And the PG pin tied a 10k Ohm to an external 3.3V.

The Iout is 2A, if the Vdrop is 0.5V, the Vout drops from 5V to 4.5V, and VFB = 90%.

By those conditions, will it cause the PG to go low?