Other Parts Discussed in Thread: LM74502
Hello Team,
We are planning to use the IC LM74502HQDDFRQ1 for one of our applications.
We have a system which is working from a 12V adapter.
The load current will be 12A maximum.
During wiring assembly, there might be chances the power supply is connected wrong and it may damage the system.
So we are looking for an over voltage and reverse polarity protection.
Can anyone suggest whether LM74502HQDDFRQ1 is a good choice for our application?.
Supply Voltage = +12V
Load current = 12A.
Device will 100% time ON.
Can you please suggest a MOSFET as well for the application?.
Looking for the reply.