Other Parts Discussed in Thread: REG710-3
I designed my circuit with REG710-3.3V (Fxied output voltage) model.
[Issue statement]
Output voltage is 1.69V when EN pin is pulled low.
** Note: When my mcu give HIGH on EN pin, 3.3V measured correctly.
Since there is Schottky diode directly on OUTPUT pin, there's no way the 1.69V would come from external load or other components.
Should it be 0V when EN is LOW?
I checked over 10 times for the circuit.