This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65131-Q1: Suggestion for split rail DCDC converter

Part Number: TPS65131-Q1
Other Parts Discussed in Thread: BUF634A

Hi

I'm looking for a solution to create a split rail supply for the BUF634A buffer.

Requirements

Vin: 24V

Vout: 8-10V (+/-)

Iout: 500mA OR 2.5A (driving 5 buffers, so separate DCDC per buffer, or common DCDC)

Temperature: -40 to 125 degC ambient

Notice: the buffer will never draw high current at both positive and negative simultaneously.

This is for an internal test platform.

Anyone have suggestions on partnumbers? (above partno closest I could find, but not correct Vin or temperature).