Part Number: TPSM365R3
Hello,
I did a Webbench simulation of TPSM365R3FRDNR using the following parameters:
- Input 14 to 26V
- Output 8.5V / 0.2A
- User prefered frequency 1.9 MHz (Rt = 8.2 kOhm)
Webbench shows a resulting efficiency of >90% for all input voltages and output current >0.15A.
Now I measured my real application with a constant load of 0.17A. The efficiency started at 85.5% @14V and dropped linear to 74.8% @26V.
What is wrong here? Is there a bug in the Webbench model?
Regards, Peter