Part Number: LMR62421
Hi there,
What is the maximum allowed output capacitor for LMR62421?
- Vin = 5V
- Vout = 12V
- IOut = 350mA
Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ais,
Usually there is a requirement on the min capacitance of the Cout, decided by the acceptable Vout ripple.
For LMR62421, a min 4.7μF Cout can cover the most applications. So 4.7μF - 10μF Cout is recommended.
What's the Cout that you'd like to use? Extremely large Cout may causes issues in start-up, loop stability and transient response.
Regards
Lei