Dear TI team,
I have some trouble in analysis with the TPS7A4501-SP (1.5A version) regarding the dropout that is mentioned in the datasheet for a vout of 19.3V. I would need a way to compute the dropout for a vout of 2.8V@100mA load.
I have the exact same issue as this post: https://e2e.ti.com/support/legacy_forums/hirel/f/space-high-reliability-forum-read-only/658334/tps7a4501-sp-dropout-for-5962r1222403vxc-1-5a-version-at-3-3v/2418553#2418553 (except i want to compute @2.8V)
But i'm unable to open a related question.
One of your expert responded via e-mail to the other guy, would it be possible to have access to those data? i have 18 of these chips in hand, and no solution to use them after our worst case analysis that use the maximum dropout voltage of 0.58V,
Thanks for your help.