Dear Specialists,
MY customer wants to know about the maximum sink current of the PG pin.
I would be grateful if you could advise.
---
①I would like to know about the maximum sink current of the PG pin.
The value of the pull-up resistor cannot be determined because it is not mentioned in the data sheet.
The pull-up resistor for the PG pin is 1MΩ in the Typical Application circuit diagram.
In the "PG output low voltage" item, the operating conditions are "VOUT = 3.3 V, IPGL = 10 μA".
For these reasons, we believe that it is necessary to select a MΩ level pull-up resistor.
Could you please let us know the maximum sink current of the PG pin.
② Regarding the voltage applied to the PG terminal, the data sheet states that the maximum rating is 7V, so we have determined that there is no problem with pulling it up to 5V.
Is it possible?
Just to make sure, I would like to check if there is no problem even if I apply 5V continuously.
---
I appreciate your great help in advance.
Best regards,
Shinichi