Other Parts Discussed in Thread: TUSB8044A, TUSB1064
Hello,
Please see my simplified Block diagram below.
I am working on the following HUB design:
INPUT: the USB-C Host (PC or Laptop)
OUTPUTS: 4x USB-C + Display Port
QUESTIONS:
1. Is the Block diagram (with TUSB1046A, TPS65983 and TUSB8044A) correct approach?
2. Since I will not use the outputs of the HUB for charging and the USB-C outputs will be very low current (I will need USB-C Host current setting for fixed value of 1.5A), could I use the simpler approach for PD Controller than TPS65983? Do you have any recommendation?
Please, see Block diagram below.
Thank you for your help.
Pavel Skoda