Other Parts Discussed in Thread: PMP22301
I'm adding dual ethernet to an existing product. POE is one of the design requirements.
The system is typically powered by 24 VDC (wall wart or similar). Total system power is no more than 8 watts.
The first search result I got was the LM5071 which is a good solution because it allows the system to be isolated from either POE or from an external DC supply, enabling customers to choose the power source (another design requirement)
But this raises a couple of questions.
Examples show 3.3 V and 5 V, but nothing higher. There doesn't seem to be a max specification for Vout. Is it okay for the output of the transformer to be 24 Volts?
Can the LM5071 handle 24V to 24V buck / boost operation from an external supply?
Thanks in advance.