This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ77915: Help me review my schematic for BQ77915

Part Number: BQ77915

I have used the following while designing

  1. Part BQ7791502
  2. Use only 3S cells.
  3. Charging voltage upto 4.1V/cell and 12.3V for the pack from the charger IC
  4. Discharging current will be 4A
  5. Balancing: Internal
  6. U42 will be the balancing connector
  7. U24, U41 - will be the positive and negative terminal of the batteries in series.
  8. 15mOhm is 0.5W rated
  9. All capacitors are 50V rated

Link to the file: https://drive.google.com/file/d/1ucfiDsUnK9SovGX9bE3WRBVPQrb_qzmp/view?usp=sharing

Thanks a lot in advance for the support!