Question 1:The picture shows the charging IC (input) charging current curve, which is BQ24010 to charge the lithium-ion battery. At 10°C, it is found that after the battery is fully charged, after turning the light, there will be uninterrupted charging, as shown in the figure, is this normal? I did not see this phenomenon at 25°C, what is the reason?
Question 2:
The data sheet of IC bq24010DRCR include many other models. The timers included in IC bq24010DRCR cannot be distinguished. May I ask which timers are included in IC bq24010DRCR? t (PRECHG)? t (TAPER) and t (CHG) ? Does t (TAPER) time timeout directly indicate charge completion rather than an anomaly?