Other Parts Discussed in Thread: LM5145
Hi team,
This is Venu Gopal.
I have an issue with IC LM5145-Q1. I have five DC-DC converter circuits in series on a PCB which are designed for 24V and 8A each. This each Converter output again divided into 5 parallel outputs each 1.5A/24V. When i checked the individual circuits i got expected output voltage at converter stage as well as at the parrel outputs. when I turned on all together only first and second circuits giving expected output voltage remaining circuits are not giving 24V. I found that MOSFET Gate and Source is shorted. Now I have changed the MOSFET's still I am not getting the output voltage. I am not getting any gate pulse at the MOSFET Gate Pin. I am attaching Schematics for your reference.
Similar five circuits in series on the PCB.