Part Number: REF3030
Other Parts Discussed in Thread: REF35, REF4132, REF3130
Hi
How to calculate the upper and lower limit of output voltage including temperature drift?
I am thinking as below, is it correct?
Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Here is how I would calculate the minimum and maximum error for -10°C to 65°C when taking only initial accuracy and temperature drift into consideration:
Temperature drift max error = 75°C * 60 ppm/°C = 4500 ppm
Initial Accuracy Max Error = (3.006 V -3 V)/3 V = 0.2% = 2000 ppm
Total max error from initial accuracy = 6500 ppm
Total voltage error = 3 V ± (3 V * 6500 ppm) = 3 V ± (3 V * 0.65 %) = 2.9805 V to 3.0195 V
In the future, there is a calculator tool that can be very helpful for this:
https://dev.ti.com/gallery/view/LPVRS/ADC-TO-VREF-SELECT_Design_Tool/ver/1.0.0/
Here is how I used it with the values you shared:

Please ensure that as you use the calculator that you are inputting the correct values from the datasheet, and are setting the parameters you are not interested in to 0, as is shown in the example above.
Using the same method by using the calculator for -30°C to 85°C, the voltage range becomes:
3 ± (3 V * 0.89 %) = 2.9733 V to 3.0267 V
If you would like a voltage reference with better temperature drift performance, you can consider options such as REF3130AIDBZR (REF3130), REF35300QDBVR (REF35), or REF4132B30DBVR (REF4132).
Thanks,
Jackson