Part Number: TPS2372-4EVM-006
Other Parts Discussed in Thread: PMP20859
Q1:If I use the FDMQ8205A(ideal diode bridge) in the TPS2372-4EVM-006, how does the FDMQ8025A block reverse current to each other?
e.g, if the signal pair input is +57V, and the spare pair input is +56V, the PMOS of Q1.pin4 is closed because its gate is low, and the PMOS of Q4.pin4 is closed too because its gate is low too. So +57V and +56V will be shorted together, I don't think the silicon diodes have this problem, Sorry I'm confused about it, so I have next Q2.


Q2: If I want to parallel two PD ports in the system, can I short the input like figure below?