Other Parts Discussed in Thread: TPS55340, TPS61040
Hello,
I wanna design Boost circuit to increas voltage to 28V by using 5V.
in case of TPS61040-Q1, possible output voltage is 28V at maximum according to datasheet.
I think, it means there are no margin when I make the circuit.
Is there any problem to make circuit like below?
R1 = 2200Kohm
R2 = 100Kohm (or smaller)
L = 22uH
(output current = under 20mA)
Thank you.