This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC14341-Q1: Maximum efficiency of 50-60%?

Part Number: UCC14341-Q1


Hi, I have checked the part efficiency (Fig. 6-18 to 6-21, Fig. 6-30 to 6-32) the efficiency is in % and the scale is 0 to 1.

- Does 0.5 mean efficiency of 50% here?

- What is the efficiency curve versus output current of this DC-DC isolated converter say if i would to have the output voltage of +15/-10V (total 25V)? I have checked all datasheets from the same product type and they are presented in the same format.

Kind regards,

Ponggorn Kulsangcharoen