Other Parts Discussed in Thread: LM66100
Hi all,
I have a setup with a TPS54331 configured to 5V output and want to OR between a primary(24V) and secondary (5V USB) power sources.
The secondary 5V-usb source in only used during maintenance to update the firmware on the board. Usually, the primary power source is disconnected during the flashing process, however the design should be capable of having both sources present at the same time.
When the secondary supply is connected and the primary is disconnected, the TPS54331 has 5V-Vd2 on its input.
What happens when the input is lower than the desired output(5V)?
The input would be over the UVLO so the IC should still be on. It is correctly understood that the output then would be input*0.9(min duty cycle)?
Do you have any advice on other ways of doing the ORing circuit?
Thank you.