Tool/software:
Hello,
I see that this IC's datasheet recommends a maximum Dx channel current of 25mA, but does state that it maxes out at 50mA if Iset is connected to Gnd.
Is connected Iset to Gnd a viable design option?
I have a design where I would like to drive two LEDs in parallel with an average of 75mA through each if I can tune some ballast resistors. It seems that I could potentially achieve this through maxing out this IC's capability.
Is that a sustainable option, or will this significantly shorten this IC's lifespan?
To add context, these LEDs will not be permanently on, but flashed in a pattern potentially up to a 50% duty cycle.
Thank You,
Wesley Mandel