This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24703: PWM Control For "CC Charge"



Hello I have Just One question

I designed as follow

1) IBAT Setting is 16A

 * VSRSET : 2V

 * Rs : 0.005ohm

2) IADT Setting is 16.8A

If I design it like this,

Starting from 16A, CC charging by PWM control

When 16.8A, Is it Stop the charging?

If it's the wrong design, What should I do?

Thank you.