Part Number: TPS5410
Tool/software:
Hi
I am working on TPS5410.
I just want to know if there is any calculator to calculate the compensation values
Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS5410
Tool/software:
Hi
I am working on TPS5410.
I just want to know if there is any calculator to calculate the compensation values
Regards
Hi Subash,
No need for compensation, the device has an internal type III compensation network inside.
You can add an additional 10pF feed forward capacitor between VOUT and FB.
Thanks,
Andrew
Hi Andrew,
Thanks for the reply
I had tested the device with 10pF as you suggested
But there is no positive results, I am getting unstable voltage at output
I tried with MLCC and Aluminum Capacitor at output, Once i get right voltage then again it goes unstable
Is there any special low ESR capacitor requirement ?
Regards
Hi Subash,
Could you post a screenshot of the relevant portion of the layout please?
Thanks,
Andrew
Hmm,
It seems like the ground loop on some of you components is not ideal. You would really want D1's ground connection to be close to the bottom terminal of the input capacitor C2.
I'd also add a 100nF input capacitor close to the VIN pin.
You could also try a lower inductance value and see if that helps, but I mainly think that if the ground connections are improved you may get a better result.
Thanks,
Andrew