Tool/software:
Hi,
I want to ask question regarding using relay (G5Q-1A4-DC12) at the switch node of half bridge circuit to connect and disconnect individual transformers contacted in parallel to the circuit. See the attached image below. The transformers are connected via relay to the floating side and in between the two capacitors that form a half bridge circuit as shown in the attached image. The relay is just to turn ON/OFF the transformer that is not required during operation. The switching frequency of the gate driver circuit is 25kHz to 39kHz.
1) Is the relay appropriate in the switch node?
2) Is there any better approach of achieving this requirement?
Kind regards,
Bright