Other Parts Discussed in Thread: UCC28180, UCC28064A
Tool/software:
Hi,
I would like to understand the lower voltage divider used for UCC28056, attached, page 28- schematic 39, 40 Resistor network divider
1) Why was the resistors connected in parallel?
2) Webench simulation shows that 3 x 3.4M upper and 66.5k ohms lower resistor network can used to get 390V output, is that correct?
3) Can I use 3x 3.4M and 66.5k ohms for the voltage divider to get 390V, it makes it easer to add a potentiometer to control the output, compared to using the parallel connections in the datasheet application example.
Kind regards,
Bright