Other Parts Discussed in Thread: TPS61288
Tool/software:
Dear TI,
I have used TPS 61178 to generate 12V of my BLDC motor via an electronic speed controller.
Here is the following crude observation I found:
1. With the input voltage of less than 4.15V (Li-ion Battery voltage) and boosted to 12V, it’s almost not possible to drive the BLDC motor even without any load
2. When I reduced the output voltage to 10V, I can boost the voltage with input voltage down to 3.6V and with the output load less than 10W
3. When the output is loaded, meaning the load increases power draw more than 10W, the boost converter resets itself.
So, if I would like to boost from 3.3V - 4.1 V to a consistent 10 - 12 V with output power upto 20 - 25W, what boost converter do you know I can use? Apparently the TPS61179 requires larger input voltage for high power output.
Separately, when the load current reaches 4A, the input voltage losses can be as big as 0.4V, which really affects the boost capability. Do you have any suggestion in the input and output traces design to handle high load current?
Thank you very much and I look forward to hearing from you,
Khoi Ly