This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61099: Enable input maximum voltage

Part Number: TPS61099


Tool/software:

Dear Sirs!

I am going to use TPS61099YFF in following conditions:

Vin 1.05-1.65V

Vout 3.3V

Question. Can enable input be connected to port of controller? Voltage is  1.8 V. It is higher then Vin. Can it cause any problems?

Please advise.

Thank you