Tool/software:
We are considering a circuit with an input voltage of 9V and an output voltage of 12V.
If the output voltage setting is 12V and the input voltage is higher than 12V (e.g. 13V), what will happen to the output voltage of the TPS61378-Q1?