Other Parts Discussed in Thread: BQ25619, BQ25616, BQ25618, BQ25618E, BQ25611D
BQ2561x FAQ Home Page
This home page is for common questions in relation to the BQ25611D, BQ25616, BQ25616J, BQ25618, BQ25619, and BQ25618E.
FAQs
------------------------------------------------------------------------------------------
Charging regulation:
- Why does ICHG reduce when reaching the maximum duty cycle?
- Why does ICHG reduce during the input current DPM (Dynamic Power Management) or the input voltage DPM?
System regulation:
- Why VSYS does not start up normally when there is a loading on the SYS and the battery is not present?
- Why does the LED connected to STAT pin flashes and the SYS voltage unstable when battery is not connected?
Battery temperature feedback and charging effects
- How does JEITA apply as it relates to charge voltage and charge current?
- How do I set the temperature range I desire using the TS pin on BQ2561x?
Safety features:
- How does the charge safety timer work?
- Why do I have to read the fault status twice to see the cleared fault on BQ2561x?
OTG function:
Ship mode + /QON Pin:
- What is ship mode and how do I enter and exit it in BQ2561x?
- What is the function of the /QON pin on BQ2561x?
Miscellaneous:
Software:
Application Notes
- Selection of Single-Cell Buck Narrow VDC Switching Battery Chargers
- Dynamic Power-Path Mgmt & Dynamic Power Mgmt (Rev. A)
- Battery Charger Overload Protection in Boost Mode Operation
- USB D+/D- Input Current Limit Detection
- High-Efficiency Charging for TWS Using a 2-Pin Interface Application Report (Rev. A)
Other Documentation
- How to choose the right charger for industrial batteries
- Powering the smart home with a simple charger
- Benefits of rechargeable batteries in real-time location system trackers
Datasheets
- BQ25618/619 I2C Controlled 1-Cell 1.5-A Battery Charger with 20-mA Termination and 1-A Boost Operation datasheet (Rev. D)
- BQ25618E, BQ25619E I2 C Controlled 1-Cell 1.5A Battery Chargers with 20mA Termination Current datasheet (Rev. B)
- BQ25616/616J Standalone 1-Cell 3.0-A Buck Battery Charger with Power Path and 1.2-A Boost Operation datasheet (Rev. A)
- BQ25611D I2C Controlled 1-Cell 3.0-A Buck Battery Charger With USB Detection datasheet (Rev. B)