This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25942A: Schematic review for TPS25942A

Part Number: TPS25942A

Tool/software:

Hi E2E team,

Please help me review the schematic and HW setting for TPS25942A.

Condition:

Vin(normal)=12V

ILimit=1.18A

V(OV)=13.25V

V(UV)=10.85V

In addition, I have the following items that I would like to consult with TI:

[1] nFLT and PGOOD

    I would like to connect these two signals to MCU. Due to power domain of MCU, I use the 1.8V for these two signals. is it ok?

[2] IMON

    I'm not sure this signal can be directly connected to the ADC pin of the MCU. if that can be happen, The RIMON resistor value must be recalculated.

    In this case, V(IMONmax) is 1.8V?

BR,

Caspar