Tool/software:
Hello,
Can you please review the design of TPS62175DQCT. I have attached a PDF file of the same.
PFA.
Awaiting for your valuable feedback
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
Can you please review the design of TPS62175DQCT. I have attached a PDF file of the same.
PFA.
Awaiting for your valuable feedback
Thanks
1. if the PG function is not used, this pin should be left open. Do not connect it to ground;
2. Recommend adding a 0.1uF ceramic capacitor on the input side, and the Cin should be placed as close to the device Vin pin and GND pin as possible.
Thanks and best regards.
As mentioned in Datasheet, PG can be left floating or connected to AGND. So, is there any specific technical reason as per my design you are trying to point out or it is still okay if we keep PG pin connected to GND ??
Thanks & Regards
Yes it's ok to keep PG connected to GND as specified in datasheet.
Thanks and best regards.