This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV431: OP temperature

Part Number: TLV431

Tool/software:

Hi team,

we are promoting the TLV431 in their solar inverter project, the operating ambient temperature of PW-TL431AIL3T SOT32-3 is -40~85℃, Customer need to do the temperature pressure test in 85℃, So they are concerned about the temperature spec. So do you have some comments about that? Is the temperature spec suitable for their requirement?

BR

Jingguo

  • Hello Jingguo,

    We guarantee the datasheet specs up for the whole rated temperature range. If the customer has concerns they can use a Q-grade part with a temperature range of -40 to 125C.

    TL431AQDBZR is pin to pin with TL431AIL3T and has the same 2.495V Vref voltage. If 1.24V vref is needed, TLVH432AQDBZR is pin to pin with a 1.24V vref like TLV431.

    Thanks,

    Walter