Part Number: TPSM843B22E
Other Parts Discussed in Thread: TPSM843820, TPSM843A22E, TPSM843A26E, , TPS543820, TPS543B22, TPSM843B22
Tool/software:
Hello:
I note that Texas Instruments has some new switcher modules that are major reductions PCB footprint from the prior generation. That's very nice as a new design option, but there do not seem to be SPICE models available yet.
The parts in question are:
- TPSM843820 with 8A output.
- TPSM843A22E with 12A output.
- TPSM843A26E with 16A output.
- TPSM843B22E with 20A output.
My questions are:
1. Are the major reductions in area (these are only 5% to 20% the PCB area of previous parts) the result in new advances in 3-D assembly? Are there new technologies in play like GaN and SiC? I'm just curious about that because it does seem to be huge advances happening over a short period of time. Is there anything published explaining these advances?
2. Are SPICE models to be made available? If so, when and in what SPICE package? If PSPICE format, will they be unencrypted so that they can be moved to LTSPICE for better convergence and speed? Will they be transient form so ripple can be simulated? Will a linearized model also be available for loop BW and phase margin simulation?
3. There is a "SIMPLIS" form model for the TPS843820. This seems to be a linear approximation (cannot sim switching noise) within the SIMetrix simulator, which is yet another version of SPICE that TI is apparently getting into. Is there a plan here for offering linear switcher models in SIMPLIS and not in the more common SPICE versions?
Thanks,
Farron