I'm using the reg710-3.3 (SOT23-6 package) in a battery powered application and see excessive quiescent current when ENA is pulled low. Should be < 1uA according to the spec, but I'm seeing up to 900uA through the reg710 when ENA is low and the output is shorted to GND. Input voltage is 3.7V nominal. Circuit is based on the reference in the spec. Any advice?
--David Gunderson, Micro Power Inc.