This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1641: Question about design calculation tool

Part Number: TPS1641


Tool/software:

Dear TI experts,

My customer checks TPS1641 design calculation tool.

Could you explain the parameters below and how can I set these values?

1. Icharge_req = Charging (inrush) current desired in the system = default is 0.10A

2. RIstart = Load at start-up (Enter an equivalent resistor value) = default is 100 ohm.

Best regards,

Chase

  • Hi Chase,

    Icharge_req is the amount of current you want to limit into the load capacitance during startup.

    RIstart  is the resistance of load.

    If load is not resistive, you can calculate as follows. For example load turn-on at 10V and draws 0.2A then RIstart = 10V/0.2A = 50 Ohm

    BR,

    Rakesh